Technical FAQs

Ask a Question

Where can I download Power Monitoring Expert 8.1 installation files?

The installation files for Power Monitoring Expert 8.1 (PME 8.1) are needed

Power Monitoring Expert 8.1 (Base, Health Care, Data Centers, and Buildings)

Software Installation Files

PME 8.1 Standard and Buildings Edition DVD (ISO) software can be found at the Schneider Electric Box links below: (PME 8.1 is a free upgrade from PME 8.0)
PME 8.1 Base
PME 8.1 Healthcare
PME 8.1 Data Center

Note: If there are issues accessing the above links, please try removing the secure encryption by removing the s in https. For example, the first link would become

For PME 8.1 Documentation, refer to article FA254980.
Was this helpful?
What can we do to improve the information ?