Technical FAQs

Ask a Question

.chm error "Navigation to the webpage was canceled"

ION Device Template Reference downloads, but when opening the .chm the display page gives the following error:

Product Line
ION Device Template Reference.chm

.chm files

User security permissions on the PC may be set to block .chm files to protect the PC.

1. Right-click IONDeviceTemplateReference.chm
2. Select Properties
3. Navigate to the General tab (if not open by default)
4. Under the Security session, click Unblock.

5. Click Apply. Then click OK.
6. Re-open the .chm and the information should become viewable.

Was this helpful?
What can we do to improve the information ?