Search FAQs
Where can I download the latest version of the software migration Configuration Manger Tool?
Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.1
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
PME Configuration Manager Tool
Resolution
*The use of this component, and any component in the Toolkit, has the potential to modify system configuration and should only be used by competent personnel. Backups of database and/or System Configurations should always be made prior to utilizing tools. Schneider Electric bears no responsibility for changes made as a result of the use of this tool. The component is posted on an as-is basis.*
As of November 2019, the latest version of Configuration Manager Tool is Configuration Manager 2020 for PME 2020, which can be found in FA402590 or inside of the PME_2020.iso file under ...\Setup\CM Tool.
This is also the case for the PME 2021, PME 2022, & the PME 2023 iso file.
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.1
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
PME Configuration Manager Tool
Resolution
*The use of this component, and any component in the Toolkit, has the potential to modify system configuration and should only be used by competent personnel. Backups of database and/or System Configurations should always be made prior to utilizing tools. Schneider Electric bears no responsibility for changes made as a result of the use of this tool. The component is posted on an as-is basis.*
As of November 2019, the latest version of Configuration Manager Tool is Configuration Manager 2020 for PME 2020, which can be found in FA402590 or inside of the PME_2020.iso file under ...\Setup\CM Tool.
This is also the case for the PME 2021, PME 2022, & the PME 2023 iso file.
Previous versions
- [PME9.0][Tool] Configuration Manager 9.0 - FA402587
- [PME8.2][Tool] Configuration Manager 2.1.0 - FA402580
- [PME 8.1][Tool] Configuration Manager version 2.0.x - FA402581
- [PME7.2.2][Tool] Configuration Manager version 1.x - FA402586
Released for:Schneider Electric Global
Attachment(s)
Explore more