Browse FAQs

Can OFS call up a direct Modbus address that has no symbol?

Published date: 10 October 2019

Issue
Need to use OFS/OPC to read 4x registers from a device that does not support symbols/variables.

Product line
OPC/OFS

Resolution
 The syntax is  Aliasname!400001 to call up address 400001.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.