Browse FAQs

Why does Power Factor not show up in Facility Expert widget even though its being published from the meter?

Published date: 28 October 2019

Issue
Power Factor widget not updating with data. Com’X is logging and publishing the parameter directly from the meter.


Product Line
EcoStruxure Facility Expert

Environment
Facility Expert widgets


Cause
Facility Expert recalculates Power Factor based on incoming Active and Reactive Energy data.

Resolution
All the Active and Reactive energy should be selected for logging and publishing in Com'X.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.