Browse FAQs

What is UMAC error "Parameter out of range (value (7999) not in [-1500 to 1500])" ?

Published date: 09 October 2019

Issue
When using the Unity M580 Application Converter to convert Quantum to X80 IO the Parameter error occurs.

Product line
Unity M580 Application Converter

Resolution
This issue existed in versions prior to 3.1.x but has been addressed.  Upgrade to the latest version of UMAC.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.