Browse FAQs

Proworx 32 pops up with a log in screen what is the login?

Published date: 27 September 2019

Issue:
What is the login password for Proworx 32 when opening a project?

Product line:
Proworx 32 and all controllers supported by it.

Environment:
Proworx32

Cause:
Getting pop up on launching program and not sure why it pops up and how to resolve.

Resolution:
This is a default setting, when the screen pops up all you have to do is remove the check mark where it says "Display dialog on startup" and then hit bypass. Once this has been don the Login pop up will no longer be displayed.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.