Browse FAQs

ATO dumps the load as the load increases

Published date: 24 September 2019

Issue:
ATO system dumps the plant load when on generator power, as the load increases

Product Line:
Premium PLC

Cause:
47 pickup is too low at 2%

Resolution:
Increase 47 pickup to 6%

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.