Browse FAQs

Assigning IP Address to Momentum with EcoStruxure Control Expert

Published date: 24 September 2019

Issue
How to assign an IP address to a Momentum PLC with EcoStruxure Control Expert software

Product Line
Modicon Momentum

Enviroment
EcoStruxure Control Expert

Resolution
1. Open or create a Momentum project in Control Expert.
2. Create a new Ethernet network
3. Open the configuration window for the Ethernet network. Select the correct Model Family. Enter IP Address that is desired.
4. Link the Ethernet network to the Momentum Ethernet port.
5. Build project and download to the PLC.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.