Browse FAQs

Why does the background color my Vijeo Designer project incorrect?

Published date: 24 September 2019

Issue:
The background color appears incorrectly in a Vijeo Designer project. The color is not as selected in the color palette.

Product Line:
Vijeo Designer (all versions)

Resolution:
When the GridXSpacing and GridYSpacing properties are both set to 1, the grid will overpower/overwrite the color of the background color of the panel. The entire panel will appear white (the color of the grid) and not the selected color for the panel. To avoid this situation, ensure the GridXSpacing and GridYSpacing properties are set to at least 10.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.