Browse FAQs

Can a Modicon PanelMate HMI project be converted for use in a modern Magelis HMI?

Published date: 23 September 2019

Issue
I would like to convert a Modicon PanelMate HMI (Legacy) project to a newer product for Magelis iPC. What product is this possible with?

Product Line
Modicon PanelMate, EcoStruxure Machine SCADA Expert

Environment
HMI Configuration Software for Windows

Resolution
Yes, this is possible.
The product line that a PanelMate HMI project can be converted to is EcoStruxure Machine SCADA Expert. EcoStruxure Machine SCADA Expert can run on Magelis iPC or Standard PC running Windows 7 or higher.

In order to be able to convert the PanelMate HMI project, it must be brought up to:
PanelMate Plus Configuration Editor - Version 4.01b0

See this guide for more details:
"EcoStruxure Machine SCADA Expert Import Tool for PanelMate, User Guide"
https://www.schneider-electric.com/en/download/document/EIO0000002707/
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.