Browse FAQs

Vijeo Designer: Is there a way to disable System Error Log Message pop-ups on an HMI?

Published date: 20 September 2019

Issue
In Vijeo Designer, how do you disable the System Error Log Message pop-ups at the bottom of the screen on an HMI?

Product Line
Vijeo Designer, Magelis HMI running Vijeo Designer Runtime

Environment
Vijeo Designer Editor on Windows PC

Resolution
Yes, the way to disable the System Error Log Message pop-ups by configuration is via the following steps:
  1.  In the Project Navigator, select the “Alarms & Events” node.
  2. Then in the last row of the Property Inspector, you will see the setting “Show System Error Window.
  3. Set that to “No” in the dropdown to the right.


It is then recommend to put in a screen that contains a System Error Log object so that  system errors can be seen by changing to this panel if desired. 
This can be found in the Toolchest -> Diagnostic folder and can be dragged onto the screen. Various sizes of the screen object can be found in the Toolchest.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.