Browse FAQs

What is the TM2AMI8HT replacement?

Published date: 18 September 2019

Issue:
What is the recommended replacement for the Twido TM2AMI8HT I/O module?

Product Line:
Twido, TM2

Cause:
Product obsolescence of the Twido and TM2 I/O lines.

Resolution:
The replacement for the TM2AMI8HT would be the TM3AI8 but, this will not work with the Twido  line or the OTB line both would need to be upgraded to the M221 product line to use any of the TM3 modules.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.