Browse FAQs

What does fault code 11 indicate on an LTMR Tesys-T product?

Published date: 16 September 2019

Issue:
Customer is experiencing a major or minor internal fault with their LTMR product.  Fault code 11 has been retrieved from the fault history.

Product line:
LTMR Tesys T

Environment:
All models and serial numbers.

Cause:
The internal temperature of the LTMR is too high and the performance of the Tesys T may be unreliable.

Resolution:
The LTMR must be allowed to cool to a normal operating temperature before reliable performance can resume.

Please see the attached file for the trigger points for the minor internal fault and major internal fault codes.  
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.