Browse FAQs

How do you create a .STM file?

Published date: 23 September 2019

Issue:
Creating a .STM file using the Unity Loader

Product line:
Unity Momentum, M340, M580, Unity Quantum.

Environment:
Unity Loader

Cause:
Unable to create a .STM file using the Unity Loader

Resolution:
To create the .stm file you have to use Unity Loader and use the following procedure

1. PC<=> PLC
2. Click on the 3 dots ...
3. Create a project name .stm
4. Connect
5. Transfer this will upload project from PLC to PC (this will create the .stm file and transfer to where you point to).
6. Close and disconnect the file has now been created
7. You can now download using Unity Loader  PC<=> PLC
8. Point to the off line .stm file
9. Open
10. Connect
11.Transfer
12. Transfer complete and Close
13. Disconnect

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.