Browse FAQs

What is the equivalent cable to the XBTZ9018 ?

Published date: 13 September 2019

Issue: 
The XBTZ9018 cable has a long lead time, is there another cable that I can use in place of the XBTZ9018


Product Line:
Magelis, XBT


Resolution:
You can use the XBTZ968 + XBTZG909 to replace the XBTZ9018

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.