Browse FAQs

How do the %MW addresses get added to the M340 CANopen PDO?

Published date: 10 September 2019

Issue
Immediately after adding an Altivar 71 to M340 CANopen the PDO did not assign %MW addresses.

Product line
Unity Pro, Control Expert, Modicon M340

Resolution
After adding the device, the project must be built in order for the %MW addresses to appear in the PDO.







 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.