Browse FAQs

What cable is needed for the BMXART0814?

Published date: 06 September 2019

Issue:
What are the cables for the BMXART0814 module and what are the lengths?

Product line:
x80 I/O, M340, M580

Cause:
Need to know what cable are needed and how long they are.

Resolution:
There are 3 lengths for the cable from the BMXART0814 module 
BMXFCA152  1.5 meters
BMXFCA302   3 meters
BMXFCA502   5 meters

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.