Browse FAQs

Why does Unity launch but stays in the Taskbar and not on the screen?

Published date: 05 September 2019

Issue
After launching Unity it is clear that it is running, but can not see it on any of the screens.

Product line
Unity Pro, Control Expert

Resolution
Had him hold down the shift key, right click on the icon in the task bar and select Move from the popup menu then use the Left/Right arrow key to move it into focus.
This is something that can happen in Windows from time to time regardless of the program that is launched.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.