Browse FAQs

What is the overvoltage level on the ATV212?

Published date: 15 September 2019

Issue:
Overvoltage level on the ATV212.

Product Line:
ATV212

Environment:
All serial numbers, all model numbers

Cause:
N/A

Resolution:
F626 is the parameter for overvoltage level.  F626 can be set between 100 to 150% of nominal DC bus voltage.  Parameter F626 sets the DC bus voltage level at which actions define by parameter F305 take place.  See diagram below for more details.


 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.