Browse FAQs

How to wire and power up the transmitter using 24Vdc on the ATV320 drive?

Published date: 15 September 2019

Issue:
Can the transmitter be wired and powered up with the internal 24Vdc on the ATV320 drive?

Product Line:
ATV320

Environment:
All serial numbers, all model numbers

Cause:
Customer had a transmitter that needs 24Vdc to power up.

Resolution:
You can use the internal power supply +24Vdc on the drive to power up the transmitter.  The +24 terminal on the control block of the drive is the internal power supply 24Vdc.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.