Browse FAQs

Can I start and stop the soft starter ATS22 30 times within 2 minutes time frame?

Published date: 22 October 2019

Issue:
Is it possible to start and stop the soft starter ATS22 30 times within 2 minutes time frame?

Product Line:
ATS22

Environment:
All serial numbers

Cause:
Customer needed to start and stop the soft starter that many times because of their applications. 

Resolution:
It is not recommended to start and stop the soft starter ATS22 that many times.  Too many starting and stopping of an ATS22 in a short time period can cause over heating issues. 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.