Browse FAQs

Can a Unity Quantum MBP_MSTR send messages through an NOC?

Published date: 28 August 2019

Issue
Need to use MBP_MSTR in Quantum but only have NOC modules.

Product line
Unity Quantum

Resolution
The MBP_MSTR can be used with the NOC modules, the programming is equal to one that would be using an NOE. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.