Browse FAQs

Will the BMXFTW301 work with the BMXEHC0800?

Published date: 26 August 2019

Issue
Looking for a pre-wired flying lead cable to use with the BMXEHC0800

Product line
Modicon X80

Resolution
Yes, this cable assembly can be used with the BMXEHC0800. The BMXFTW301 is simply a BMXFTB2020 with flying lead 24 AWG wires.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.