Browse FAQs

M580 HSBY - Can a BMXEHC0x00 be added using CCOTF?

Published date: 22 August 2019

Issue
The existing EHC modules can be edited using CCOTF, but a new module can not be added? Is this by design?

Product line
Modicon M580, Modicon X80

Resolution
The ability to add and remove modules is limited to basic Analog and Discrete IO.  This is something that was decided during the design phase of CCOTF.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.