Browse FAQs

Is there a way to detect a broken wire on the TM3AM6 using Machine Expert Basic ?

Published date: 16 August 2019

The operating status of each I/O channel is given by the diagnostic bytes in the I/O Mapping tab:

%IWSx.y for input channel y of module x



%QWSx.y for output channel y of module x.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.