Browse FAQs

Which System Word in Machine Expert - basic can I use to indicate an I/O card is present or missing?

Published date: 16 August 2019

%SW120 Expansion I/O module status.
 
Bit 0: Reserved for the logic controller
 
  • 0 = Module is present and no error detected
  • 1 = Module not present or error detected.  The I/O expansion bus does not start unless the corresponding bit in %SW119 is set to TRUE (indicating the module is marked as optional). 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.