Browse FAQs

What is the parameter F707 on the ATV212 drive?

Published date: 22 October 2019

Issue:
What is the parameter F707 being used on the ATV212 drive?

Product Line:
ATV212

Environment:
All serial numbers

Cause:
N/A

Resolution:
F707 is local mode speed reference step that can be set to 0 (disable) or 1 (enable). 
If parameter F707 is disabled or 0 in local mode, the drive's speed reference will change in steps of 0.1Hz each time the UP and DOWN key is pressed.
If parameter F707 is enabled or 1 in local mode, the drive's speed reference will change in steps equal to the setting of F707 each time the UP and DOWN key is pressed.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.