Browse FAQs

What are the hardware and software requirements for EcoStruxure Machine Expert V1.1?

Published date: 15 August 2019

Issue:
Hardware and software requirements for
EcoStruxure Machine Expert V1.1

Product Line:
All M241, M251 and M262 controllers

Environment:
EcoStruxure Machine Expert (formally known as SoMachine)

Resolution:

This software can be installed on a personal computer with the following hardware:
• Processor Core 2 duo or higher
• RAM Memory 4 GBytes minimum, 8 GBytes recommended or higher
• Hard Disk 8 GB for typical and 15 GB for full software installation
• Display 1280 x 1024 resolution or higher
• Peripherals Mouse or compatible pointing device
• Peripherals USB interface
• Web access Web registration requires Internet access

Supported operating systems:
• Microsoft Windows 7 SP1 Professional Edition (64 Bit)
• Microsoft Windows 8.1 Professional Edition (64 Bit)
• Microsoft Windows 10 (64 Bit) 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.