Browse FAQs

Can the firmware on the VW3A3309 be upgraded in the field?

Published date: 08 August 2019

Issue:
Firmware upgrade on DeviceNet card VW3A3309

Product line:
Altivar 61 Altivar 71 Device Net

Environment:
VW3A3309

Cause:
Older firmware versions

Resolution:
No, the card firmware cannot be upgraded.  Order a replacement card with the currently available firmware.
The only firmware version is V1.1 IE04
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.