Browse FAQs

What does error 1633 mean when downloading a project to the PLC using Concept software?

Published date: 25 July 2019

1633
Checksum error
Bad communication or interruption on the line.
  • Check that the Modbus cable pinout is correct.
  • Modbus cable connected to Modbus Plus port?.
  • Try Modbus Plus or Ethernet comm.
  • Switch to ASCII mode
  • XMIT block taking port 1?
  • Download in increments.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.