Browse FAQs

What type of metal is the VW3A93111 mounting plate made of?

Published date: 25 July 2019

Issue:
What is the metal composition of the VW3A93111?

Product Line:
VW3A93111

Environment:
All

Cause:
Documentation 

Resolution:
The composition reference of VW3A93111 is: DX51D + AZ150-A-S 

DX51D: is the code for steel 
AZ150-A-S: is the description of surface treatment applied 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.