Browse FAQs

What are the Catalog numbers for the Accusine Lug Kit?

Published date: 29 July 2019

Issue
What are the Catalog numbers for the Accusine Lug Kit?

Product Line
Accusine PCS+ active harmonic filter

Environment
Hardware component
Connection accessory
Spare part

Cause
Need the part numbers for the accessory Lug kit for the Accusine PCS+ active harmonic filter.

Resolution
Lug Kit Part Number Used For
PCSPNHA45232 60 A Chassis
PCSPNHA45233 120 A Chassis
PCSPNHA50587 40 A to 120 A Enclosures
PCSPNHA45234 133 A to 300 A Enclosures
2 AWG to 350 MCM
PCSPNHA45235 133 A to 300 A Enclosures
300 MCM to 750 MCM
PCSPNHA50577 200 A or 300 A Chassis
NOTE: Phase wires and ground wires specified for the lug kits are customer supplied.

For the Lug Kit Connection Instructions see FA379196.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.