Browse FAQs

Are the TMC2 input and output cartridge modules for Modicon M221 PLCs electrically isolated?

Published date: 16 July 2019

Issue
Are the TMC2 input and output cartridge modules for Modicon M221 PLCs electrically isolated?

Product Line
Modicon M221 PLCs

Catridge modules:
TMC2AI2
TMC2AQ2C
TMC2AQ2V
TMC2CONV01
TMC2HOIS01
TMC2PACK01
TMC2SL1
TMC2TI2

Environment
Analog I/O Modules

Resolution
The TMC2 analog input and output cartridge modules are not electrically isolated between the input/output and the internal logic or supply voltage.
For electrically isolated analog input and output modules (500VAC between input and internal logic, 1500VAC between input/output and supply), please use the TM3 Analog I/O Modules.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.