Browse FAQs

Are Magelis iPCs upgradeable from Windows Embedded Standard 2009 (based on Windows 7) to Windows 10?

Published date: 15 July 2019

Issue
Are Magelis iPCs upgradeable from Windows Embedded Standard 2009 (based on Windows 7) to Windows 10?

Product Line
Magelis iPC

Environment
Windows Embedded Standard 2009 / Windows 7

Resolution
Windows 10 disk image versions of Magelis iPCs that were manufactured and sold with Windows Embedded Standard 2009 or Windows 7 from the past are not provided by Schneider Electric.
The only way to upgrade the device is by manually installing Windows 10 from a purchased Windows 10 OEM license.
The hardware drivers for the specific iPC may not be supported in Windows 10 and would solely be the responsibility of the person upgrading the device to ensure compatibility on a model-by-model basis.
It is recommended that a new Magelis iPC with Windows 10 IoT be purchased to replace the obsolete one.
For recommended replacements, please contact Schneider Electric Tech Support.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.