Browse FAQs

Where can the Modbus TCP Communication DTM Library V2.6.12 be located.

Published date: 12 July 2019

Issue
Working with a Unity / Control Expert project that has that has this DTM version and can not build the project.

Product line
Control Expert, Unity Pro, Altivar, M340

Resolution
Installing SoMove V2.7.5 will install the Modbus TCP Communication DTM v2.7.5

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.