Browse FAQs

Does the Zeliologic smart relays maintain the timer count while powered down?

Published date: 02 July 2019

Issue:
Has a timer program and may be times where the control power is removed. 

Product line:
SR2 SR3 Zelio Logic Smart Programmable Relays

Environment:
All models with time clock

Cause:
Power loss

Resolution: 
Models with the time clock have an internal battery to maintain the time/date feature so they will retain the current value in the timer when power is removed and then continue counting when power is restored.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.