Browse FAQs

Osisense XC - Where are indicated the commercial reference and the manufacture date on the ZCE10 plunger head

Published date: 27 June 2019

On the ZCE10 plunger head, such as the other ZCE* heads, the commercial reference and the manufacture date are indicated on the product : under the plunger holder on the retaining disk. See attached picture showing where are marked the head reference and the manufacture date or date code.

Was this helpful?

What can we do to improve the information ?