Browse FAQs

What is MBP_MSTR error 6007 for Unity Quantum?

Published date: 26 June 2019

Issue
Trying to send a Modbus TCP message out of the Unity Quantum native port and getting error 6007.

Product line
Unity Pro, Control Expert, Unity Quantum

Resolution
The routing register of the MBP_MSTR control word needs to be set to 16#FE00 or DEC=65024 and NOT 16#FE which is DEC=254.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.