Browse FAQs

Can the Process Drive Relay (R1, R2 etc) be configured for Frequency Threshold Attained

Published date: 25 June 2019

Issue:
Can the Process Drive Relay (R1, R2 etc) be configured for Frequency Threshold Attained

Product Line:
Altivar Process Drive

Environment:
ALL

Cause:
Wiring / Programming

Resolution:

Set R3 for [Mot Freq High Thd] FtA  then in 
[Complete settings] [Generic functions] [Threshold reached] > Motor frequency threshold ([Motor Freq Thd] FTD) reached

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.