Browse FAQs

Preventa XCS - XCSE7312 wiring diagram, visible on the front cover of the product

Published date: 24 June 2019

Find attached the wiring diagram of the XCSE7312 safety switch, having 2NC + 1NO main contacts and 1NC + 1NO electromagnet contacts. It is a version with locking by electromagnet on de-energization. The electromagnet contacts are represented electromagnet not energised. Such diagram is indicated on the front cover of the switch. The references XCSE7311 & XCSE7313 use it too. It is possible to identifiy a switch reference by this diagram, except the electrical cable entry.

Was this helpful?

What can we do to improve the information ?