Browse FAQs

On the ATV630 and ATV930, which option should I select under HMI command in SoMove to switch between terminal or HMI on the keypad?

Published date: 02 July 2019

Issue:
On the ATV630 and ATV930, which option should I select under HMI command in SoMove to switch between terminal or HMI on the keypad? 

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
Customer didn't want to change on the keypad.

Resolution:
In SoMove, select "Cmd/ref copied c/over" under HMI command.  
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.