Browse FAQs

Can I connect both computer and ATV630 or ATV930 drives to the HMI at the same time?

Published date: 03 July 2019

Issue:
Can I connect both computer and ATV630 and ATV930 drives to the HMI at the same time?

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
N/A

Resolution:
It's not possible to connect computer and ATV630 or ATV930 at the same time to the HMI.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.