Browse FAQs

How to configure a M221 analog cartridge using Ecostruxure Machine Expert Basic software.

Published date: 26 June 2019

Issue
Configuring a TMC2TI2 analog cartridge

Product Line
M221

Environment
Ecostruxure Machine Expert Basic (formally SoMachine Basic)

Resolution
1) Change the default controller type to a "C" type controller by right clicking on it and dragging over existing controller and drop.
2) Select the M221 cartridge pull down and select the cartridge you want to add, drag and drop on controller once highlighted. (for this example we will use the TMC2TI2).
3) Go to the analog input and configure from the pull down menu. Can select type and scope long with filter and comments.
4) Save and close
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.