Browse FAQs

Preventa XCS - How to order the XCSZR59010 or XCSZR5902 magnetic switch

Published date: 12 June 2019

Find attached the picture of the part XCSZR59010 which is not sold in spare parts. This part is sold under complete magnetic switch XCSDMR59010. This is the commercial reference to order to get the XCSZR59010 detector and the XCSZR1 magnet, sold into the same packaging plastic bag. For the XCSZR5902, you have to order the XCSDMR5902 = XCSZR5902 part + XCSZR1 magnet. Both references XCSZR59010 & XCSDMR5902 are available to order in 2019.

Was this helpful?

What can we do to improve the information ?