Browse FAQs

What ports does SoMove use?

Published date: 06 June 2019

Issue:
What ports does SoMove use?

Product Line:
SoMove software

Environment:
SoMove

Resolution:
SoMove ports are the following: 
Ethernet - port 502 
Modbus serial - ports 27700...27703 
Bluetooth - ports 27700...27703 (in fact, it's Modbus serial via Bluetooth's virtual COM port) 
CANopen - ports 27700...27703 and port 27800 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.