Browse FAQs

Is there a range when changing the password from the front panel of ION7330 meter?

Published date: 22 July 2019

Issue
The ION7330 meter did not save the new password when changed from the front panel. Gave error message: “New Password out of Bounds”.

Product Line
ION7300 Series Meters

Environment
ION7330 meter
ION7350 meter

Cause
The ION7300 series meters do not accept password changes above 60000 from the front panel.

Resolution
The ION7300 series meters have '00000' as factory default password which can be changed to a five digit long password with a range of '00000' to '60000' from the front panel.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.