Browse FAQs

With SoMachine, can I run the simulator and connect to the loop back address?

Published date: 23 May 2019

Issue:
With SoMachine, can I run the simulator and connect to the loop back address?

Product Line:
SoMachine

Resolution:
SoMachine simulator does not allow to connect directly using the loop back address. 
But you can connect to the SoMachine simulator by using the SoMachine protocol, where the node name of the simulator is equal to the PC device name
Make sure the SoftSPS and the SoMachine simulator are not running on the PC at the same time. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.