Browse FAQs

Is the ATV340 series drive capable of positioning by Encoder feedback?

Published date: 20 May 2019

Issue:
Customer wants to use an encoder feedback system on an ATV340 drive to allow it to turn to a specific position.

Product Line:
ATV340

Environment:
All

Cause:
Clarification of product capabilities.

Resolution:
Currently. as of 5/20/19, the ATV340 series drives are not capable of positioning by encoder.  They will require logic inputs from sensors for the positioning function.   There is a firmware evolution being developed that will enhance the positioning function.  Details of the enhancements are not currently available.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.