Browse FAQs

Osisense XC - Cross of the obsolete XCKJ567 limit switch

Published date: 15 May 2019

The obsolete XCKJ567 limit switch reference is no more available in 2019 as a complete limit switch. It has to be ordered by the sub-assemblies ZCKJ5 body + ZCKE67 steel roller plunger. Alternative is to select XCKJ part number with another cable entry like the XCKJ567H7 (cable entry 1/2"NPT) or XCKJ567H29 (cable entry ISO M20), available to order


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.